Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The following table gives an overview of all settings options. The sub-chapters give more in-depth information for certain keys.
Usually you make adjustments in the Category CAD integration -> SolidWorks. In some cases, if you want to use complex syntax, then make the adjustments in the Category Configuration files -> $CADENAS_SETUP -> ifsolidworks.cfg.
The following table gives a good overview of all keys and contains references to specific in-depth chapters. In addition you can see which features in PARTsolutions V8.1 were configured in which configuration files.
Configuration file V8.1 | Key V8.1 | |||||||
Valid path for output generation
|
pref.vbs |
See option dialog in interface menu in tab "General" -> "Store file (pool path)" |
||||||
--- | --- | --- | pref.vbs | pref.flatpool | ||||
N.A. | N.A. | |||||||
Name for file in pool directory See also Section 2.2.2, “Set file name ("FileName" key) and pool path ("poolpath" key) ” |
Different concepts (see Section 5.7.4, “Naming rules for CAD file names ”; the V8.1concept should no longer be used in V9!) |
--- | ||||||
Definition, where the material information is from. May be combined with material mapping (internal PARTsolutions material name : CAD-System material name). General information about this concept can be found under Section 2.2.5, “Material mapping ”. |
||||||||
Name of the material file from which the part material was loaded |
pref.materialDbFile | |||||||
|
||||||||
AttributeMapping(3D) | Any string |
See Section 2.3.7.2.1.1, “Declare prefix for PARTsolutions attributes ” |
pref.prefix | |||||
pref.vbs |
see options dialog in interface menu in tab "General" -> "Template files" |
|||||||
pref.vbs |
see options dialog in interface menu in tab "Parts" -> "Take over part color from template file" |
|||||||
pref.vbs | pref.connpointfolder | |||||||
pref.vbs |
see options dialog in interface menu in tab "Parts" -> "Create configurations for LODs" |
|||||||
pref.vbs | pref.creatematereference | |||||||
N.A. | N.A. | |||||||
pref.vbs | pref.multibodysolid | |||||||
Use all connection points, even for "Piping" | N.A. | N.A. | ||||||
0-2 |
1: ConstrainAll + Autodimension "1" is very slow for complex sketches! => Only use with small sketches! |
pref.vbs |
see option dialog in interface menu in tab "Parts" -> "Sketches" |
|||||
pref.vbs |
see option dialog in interface menu in tab "Miscellaneous" -> "Create assembly connection from PARTdataManager" |
|||||||
pref.vbs |
see option dialog in interface menu in tab "Miscellaneous" -> "Insert parts in active assemblies" |
|||||||
pref.vbs |
see option dialog in interface menu in tab "Miscellaneous" -> "Create assemblies as flexible components" |
|||||||
N.A. | N.A. | |||||||
N.A. | N.A. | |||||||
Interface | HoleFeatureLevel | 0/1 | Create hole in part (0) or in assembly (1) | ??? | ||||
NativeCheckin | IgnoreCheckinAttributes | CADENASIDSTR |
Exclude listed attributes at Native Checkin (several comma separated) |
N.A. | N.A. | |||
Batch | RestartCounter | 1 to N | N.A. | |||||
Batch | Mode | 0/1 | N.A. | |||||
--- | --- | --- | Obsolete for V9. The CAD system does not need to be opened from within the interface in order to export. Exporting is now always possible | pref.vbs | pref.remotecadconnection |
-----------------------------------
Configuration file V8.1 | Key V8.1 | ||||
UI |
Configuration of the PARTsolutions
interface menu and the interface toolbar occurs in the CAD
encompassing configuration file ifacecommon.cfg or the
CAD specific configuration file respectively in block [UI]. General
information can be found under Section 2.2.1.7, “Configuring
PARTsolutions interface menu and toolbar
”. |
||||
0/1 |
Exclude cutting in the 2D view for connection elements such as screws, nuts, rings, pins, etc.[a] See also Section 2.2.7.1, “NoSection ”. |
||||
[a] Default is set in ifacecommon.cfg. However via CAD specific configuration file the entry can overwritten (if needed). |