Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
All CAD specific settings can be found under PARTadmin -> Category Configuration files -> $CADENAS_SETUP -> ifugnx.cfg.
The following table gives an overview of all settings options:
See also Section 2.2.2, “Set file name ("FileName" key) and pool path ("poolpath" key) ” |
|||
Exclude cut in 2D view for connection elements such as screws, nuts, rings, pins, etc. [a]See also Section 2.2.7.1, “NoSection ”. |
|||
Valid path for output generation See also Section 2.2.2, “Set file name ("FileName" key) and pool path ("poolpath" key) ”. |
|||
CreationOptions | PipingConnPoint | 0/1 | |
Interface | NativeCheckinKey | Default: UG | Key for native check-in (CAD identifier) |
Interface | UseDefaultColors | 0/1 (Default=1) | |
Interface | ForceCreateNew3DPreviews | 0/1 (Default=0) |
Use existing "Facet Bodies" for 3D preview and geometrical search (quicker) or create new ones (more precise)?[b] |
NativeCheckin | IgnoreCheckinAttributes | Default: PSOLPARTIDENT_0_ |
Exclude listed attributes during Native Checkin (several comma separated) |
NativeCheckin | ProcessDocumentState | Behavior of the interface at Native Checkin, namely at parts, which have not been saved yet. See Section 2.3.4.1.2, “NX - Different modes at Native Checkin ”. | |
Path where to store menu file. Must be part of the "custom_dirs" files |
|||
[a] Default is set in ifacecommon.cfg. However via CAD specific configuration file the entry can be overwritten (if needed). [b] #45753 |