Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
All CAD specific settings can be found under PARTadmin -> Category Configuration files -> $CADENAS_SETUP -> ifosdm.cfg.
The following table gives an overview of all settings options:
Display name of result element (possibly different from file name) |
|||
Object name for CoCreate Modeling element See also Section 2.2.2, “Set file name ("FileName" key) and pool path ("poolpath" key) ”. |
|||
CreationOptions(is3d) | PoolPath | Local pool path | Local pool directory. This storage place is only used, when entry is set. |
Exclude cut in 2D view for connection elements such as screws, nuts, rings, pins, etc.[a] See also Section 2.2.7.1, “NoSection ”. |
|||
0/1 | |||
Storage path for native checkout files. Because CoCreate Modeling does not work with the "real" pool, a temporary directory is chosen here |
|||
Shows up after part has been inserted in CoCreate Modeling, automatic placement dialog. See also Section 2.3.2.1.2, “PositionDialog - Placement method ”. |
|||
Substitute characters, which replace the invalid characters See also Section 2.3.2.1.4, “replace_char - replacement of characters”. |
|||
Interface | ClassName |
Class name which is given for the part.
|
|
[a] Default is set in the ifacecommon.cfg. Via CAD specific configuration file the entry can be overwritten (if needed). |