Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The following table gives an overview of all keys and contains references to corresponding in-depth chapters. In addition, you can see from the table in which configuration files the corresponding features were configured in PARTsolutions V8.1.
Usually you make settings in the Category CAD integration -> Inventor. In special cases, if you want to use complex syntax, make changes in the Category Configuration files -> $CADENAS_SETUP -> ifadeskinv.cfg.
Configuration file V8.1 | Key V8.1 | |||||||||
|
pref.vbs |
see options dialog in interface menu in "General" tab -> "Data storage (Pool path)" |
||||||||
CreationOptions | PoolPath |
Is controlled directly via the setting of the pool path in V9. |
pref.vbs | pref.flatpool | ||||||
CreationOptions | Valid library directory from Inventor | See also Section 2.3.3.1.2, “ PARTsolutions pool path ” | pref.vbs | pref.projectpath | ||||||
See alsoSection 2.2.2, “Set file name ("FileName" key) and pool path ("poolpath" key) ” |
Different concepts (see Section 5.7.4, “Naming rules for CAD file names ”; the V8.1concept should no longer be used in V9!) |
--- | ||||||||
|
||||||||||
AttributeMapping |
Prefix for standard attributes. See Section 2.3.3.2.1.1, “Declare prefix for PARTsolutions attribute ” |
pref.vbs | pref.attributePrefix | |||||||
Definition, where material information comes from. May be combined with material mapping (internal PARTsolutions material name : CAD system material name). General information about the concept can be found hereSection 2.2.5, “Material mapping ”. |
||||||||||
CreationOptions | pref.vbs | pref.bomlang | ||||||||
N.A. | N.A. | |||||||||
pref.vbs |
see options dialog in interface menu in tab "Parts" -> "Forbid editing of parts (=Inventor catalog parts)" |
|||||||||
Create derived parts/assemblies See also Section 2.3.3.1.5, “ CreateDerivated(is3dPart) or (is3dasm)”. |
pref.vbs |
see options dialog in interface menu in tab "Parts" -> "Create derived parts" |
||||||||
Create a dwf file with the same name as the current document |
pref.vbs |
see options dialog in interface menu in tab "Miscellaneous" -> "Save documents additionally as DWF" |
||||||||
The activation simplifies insertion of screws, nuts, rings, washers, bearings and retaining rings. See also Section 2.3.3.1.6, “ CreateIMates”. |
pref.vbs |
see options dialog in interface menu in tab "Miscellaneous" -> "Create iMates" |
||||||||
pref.vbs |
see options dialog in interface menu in tab "Miscellaneous" -> "Apply assembly relationships from PARTdataManager" |
|||||||||
N.A. | N.A. | |||||||||
N.A. | N.A. | |||||||||
pref.vbs |
see options dialog in interface menu in tab "Parts" -> "Fix all sketches" |
|||||||||
Name of a valid template file. Via default werden the files integrated in inventor are used. |
pref.vbs |
see options dialog in interface menu in tab "General" -> "Templates" |
||||||||
threadtable.cfg | ANSI_INCH | |||||||||
threadtable.cfg | ISO_FORMING | |||||||||
threadtable.cfg | ISO_METRIC | |||||||||
threadtable.cfg | ISO_PIPE | |||||||||
threadtable.cfg | ISO_TRAPEZ | |||||||||
threadtable.cfg | XLS_NAME | |||||||||
N.A. | N.A. | |||||||||
N.A. | N.A. | |||||||||
N.A. | N.A. | |||||||||
N.A. | N.A. | |||||||||
Batch | RestartCounter | 1 to N | N.A. | N.A. | ||||||
Batch | Mode | 0/1 |
In the batchmode (1) all documents are closed automatically. |
N.A. | N.A. | |||||
NativeCheckin | IgnoreCheckinAttributes | CADENASIDSTR |
Exclude listed attributes during Native Checkin (if there are several, then comma separated) |
N.A. | N.A. | |||||
--- | --- | --- | Obsolete in V9. The CAD system must no longer be opened from within the interface in order for an export to take place. An export is always possible. | pref.vbs | pref.remotecadconnection |
-----------------------------------------
Configuration file V8.1 | Key V8.1 | ||||
UI |
Configuration of the PARTsolutions
interface menu and the interface toolbar occurs via the CAD
encompassing configuration file ifacecommon.cfg or the
CAD-specific configuration file respectively in block [UI].
General information can be found under Section 2.2.1.7, “Configuring
PARTsolutions interface menu and toolbar
”. |
||||
0/1 |
Exclude cut in 2D view for connection elements such as screws, nuts, rings, pins, etc.[a] See also Section 2.2.7.1, “NoSection ”. |
||||
[a] Default is set in the ifacecommon.cfg. However via CAD specific configuration file the entry can be overwritten (if needed). |