Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
5.8.4.
Catalog update with ERP integration - Update manager
5.8.4.6. Background
information
|
|
---|---|
Prev | Next |
Fig. „Diagram: Workflow - Catalog Update “ shows the procedure at an catalog update.
Project path, Project name and Standard number are checked for changes.
If projects have been cancelled, this is identified by the version number of the old project.
If a newer version has been added, this is identified by the version number of the old project and a new project is created.
If it is not possible to find a relation to an existing project, a new project is created.
The points 1 and 2 are basically performed, even if there is no ERP integration.
Comparison of the project lines (especially this point is part of Section 5.8.4, “ Catalog update with ERP integration - Update manager ”)
"Additional project lines" (see diagram) cannot have a link in the LinkDB. No further checking is processed.
At all project lines, which have a link in the LinkDB, an exact checking of changes (project, table, geometry) can be processed.
Furthermore the values in the LinkDB columns "ACTIVE_STATE" and "REQUESTED_STATE" are adjusted.