![]() |
In the block AttributMapping(is3d) you can determine whether the PARTsolutions standard attributes are to be transferred to the CAD system, and if so, in which language(s)
Under Attr_CopyFrom_01 set the desired language.
Assign language (german, english, french, etc.): The standard attributes are exported in the indicated language.
![]() |
Note |
---|---|
If there is no translation for selected language of the attribute, no attribute is exported (not even from the $CADENAS_LANGUAGE language). |
No entry: No standard attributes are transferred. (In order to explicitly export specific attributes, please see the information in the following sections.)
Possible values for the language are:
default,german,english,italian,french,spanish,portuguese,czech,slovak,hungarian,slovenian,dutch,danish,finnish,russian,japanese,korean,chinese,polish
For copying attributes the parameters var_exclude and var_visbile=1can be used.
var_visible=1 at this place tells the interface that only visible attributes have to be processed
With „var_exclude“ you can assign certain attributes to an "Ignore" list.
Attr_CopyFrom_01=default,var_exclude=A,var_visbile=1
The variable A is explicitly set to the ignore list.
Attr_CopyFrom_01(isCatalog(norm))=default,var_exclude=D,var_visbile=1
Here, the expression is only applied to the standards catalog.
The keys Attr_Content_01 and Attr_Section_01 remain unchanged.
In Solid Edge the attributes are displayed under Part properties on the User-defined tabbed page as standard attributes.