![]() |
2.3.5.3.
Block [UI] - Adjust menus and toolbars
2.3.5.3.1.
Application-sensitive PSOL
Ribbons
|
|
---|---|
Prev | Next |
As of V11 SP5
PSOL Menus and Ribbons will look differently depending on the currently
active NX application, namely, when no part is loaded in session, the
part-related buttons (like Execute Geometric Search). Once a part is loaded, the full menu will become
visible. This change affects all supported NX versions (8-12) and also
applies to toolbars and ribbons in versions where they can be created
(8-10 and 9-12, respectively).
This is
facilitated by a second PSOL menu, PARTsolutionsNoPart.men
file, which
contains only buttons with the app
flag attached to them in
ifugnx.cfg
file.
Both menu
files will now be placed in the application
NX folder. The
startup
NX folder
will now contain a PSOL
.men
file as well. This file will contain a list of
applications where the PSOL menus are to be shown. This list can be
accessed and modified through the PrepareMenuAppList
in
ifugnx.cfg
, directly
under the other PrepareMenu
keys. It is
prepopulated with the following NX applications: gateway, modeling, drafting,
mechatronics, route, cam, mtb, route_mech, route_elec
. You
don't need to remove applications from this list if you don't have the
license for them, or they are not installed. In this case, the entries
will simply be ignored.