![]() |
In this example Thick Lines shall be applied on layer AM_0 in Red.
Layer configuration in AutoCAD
In the Layer-Manager the layer "AM_0" is set on white.
Layer configuration in the configuration file
In the configuration file, at layer Layer "AM_0", the line color is also set to 7=White.
;----- Layer Configuration ----- ;Thick Solid Lines AcadLayerName_00=AM_0 AcadLayerLineType_00=Continuous AcadLayerLineColor_00=7 AcadLayerLineWeight_00=50 AcadLayerVisibility_00=1
Changing color by special Shape configuration
Under "AcadShapeLayer" you can see, on which layer the special Shape configuration refers.
The values for Line type, Line weight and Line color are set to bylayer by default. . Thus, the reference is to the layer configuration.
However you can explicitly specify another value of color in the Shape configuration and so override the layer configuration.
;----- Shape Configuration ----- PSolShapeType_02=0 PSolShapeWidth_02=3 PSolShapeCosmetic_02=0 AcadShapeLayer_02=AM_0 AcadShapeLineType_02=bylayer AcadShapeLineWeight_02=bylayer AcadShapeLineColor_02=1
Now after export the Thick Lines are depicted in red color in AutoCAD.