![]() |
Allocations of symbols, applications, etc. to Document types
Small symbol / Large symbol: These symbols can be used for the project view. (Acroread etc...)
Application (WIN) / Application (UNIX): File path to program file:
![]() |
Note |
---|---|
Do not forget to set "'spaces'%1" as additional parameter behind the directory information! (Placeholder for file) |
The DDE commands serve for controlling the external programs under Windows. Under Unix, DDE has no meaning.
Copy symbol files to $CADENAS_SETUP: The symbols applied under Small symbol and Large symbol become generally accessible for PARTsolutions-User.
![]() |
Note |
---|---|
The settings dialog for the Document types is also available in the PARTdataManager under Extras -> Settings... -> Part selection. See also Section 3.1.20.6.1.2.23, “ Create document project ” in PARTsolutions / PARTcommunity4Enterprise - User manual. |