![]() |
The material name must be identical to some of the names in the material table (File -> Properties -> material properties).
Per default the key is a complex vbs expression. It may be adjusted as desired.
?context.TranslateStringInGlobalOptionArray("MATMAP","",GetObject("iface.calcnameservice").start(0).Format("<CLASSPROP(cns,CNSPHYPROP,CNSMAT)>").value())
Alternative example for the vbs expression:
?GetObject("iface.calcnameservice").start(0).Format("<CLASSPROP(cns,CNSPHYPROP,CNSMAT)>").value()
Definition, where the material information is from.
May be combined with material mapping (internal PARTsolutions material name : CAD-System material name).
Material mapping is used in order to map the internal PARTsolutions material name onto the CAD system material name.
![]() |
Note |
---|---|
The untranslated name of the material is transferred; in other words the same one for all languages. |
Per default the material name is taken from the CNS classification.
When using an ERP integration the column for material is "MAT_NAME". Details can be found under Section 2.2.5.2, “Material mapping with ERP integration ”.
When using no ERP integration the column for material is "CNSMAT". Details can be found under Section 2.2.5.1, “Material mapping without ERP integration ”.
The determined name is then mapped along with the material table under block [MatMap] to the CAD system material names.
[MatMap] lead=Blei copper=Kupfer phenolic=Phenol silicone=Silikon Brass, Soft Yellow=Messing Nylon-6/6=Nylon, allgemein
Detailed information on material mapping is found under Section 2.2.5, “Material mapping ”.