Categories must be applied in the block [Categories].
In the
configuration file ifacecommon.cfg
standard categories
are already applied that cannot/should not be changed. These categories are
used in each CAD specific configuration file.
Example for the use of standard categories "is3d" in the pool path key:
poolPath(is3d)=$CADENAS_DATA/pool/solidworks
Own categories are
applied in the CAD
specific configuration files (ex. ifugnx.cfg
) in the block
[Categories].
These can the be used in as many other blocks of the CAD specific configuration files.
Below you can see
an example from the configuration file ifugnx.cfg
. First, the categories
nx4, nx5, nx6, nx7 and nx80 are defined. Then these are used for the
allocation of the fitting templates.
[Categories] nx4=GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="400" nx5=GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="500" nx6=GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="600" nx7=GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="700" nx75=GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="750" nx80=GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="800" tcActive=GetObject("iface.contextservice").GetVariable("UserApp").GetObject ("iface.teamcenter").isTeamcenterActive() [CreationOptions] TemplateName(nx4,isMMDoc)=$CADENAS/iface/unigraphics/shared/nx4/seedparts/ups_seed_mm.prt TemplateName(nx4,isInchDoc)=$CADENAS/iface/unigraphics/shared/nx4/seedparts/ups_seed_in.prt TemplateName(nx5,isMMDoc)=$CADENAS/iface/unigraphics/shared/nx5/seedparts/ups_seed_mm.prt TemplateName(nx5,isInchDoc)=$CADENAS/iface/unigraphics/shared/nx5/seedparts/ups_seed_in.prt TemplateName(nx6,isMMDoc)=$CADENAS/iface/unigraphics/shared/nx6/seedparts/ups_seed_mm.prt TemplateName(nx6,isInchDoc)=$CADENAS/iface/unigraphics/shared/nx6/seedparts/ups_seed_in.prt # etc.
The same for Solid
Edge in the configuration file ifsolidedge.cfg
looks like this:
[Categories] st1=GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="100" st2=GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="200"
And for Pro/E in
the configuration file ifproewildfire.cfg
like this:
[Categories] wf3=GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="3" wf4=GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="4" wf5=GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="5" wf6=GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="6" wf34=(GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="3")OR (GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="4") wf567=(GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="5")
OR (GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="6")
OR (GetObject("iface.contextservice").GetVariable("UserApp").cadVersion="7")
The handling of FileName often varies from one firm to another. Often the maximum length of file name is restricted by a certain system, whereas others want to have the ID in the file name, and still others do not set value upon the material in the file name, etc.
The following is a little example of how the ERP_PDM_NUMBER can be set - if available and how to define the fallback if it is not available.
FileName(isCreaOptNotSet,is3dpart)=?_FORMAT_0("<GENNAME><MATERIAL(_)>").toFileName("_").add(".ipt").value() FileName(isCreaOptNotSet,is3dpart,hasAttr(ERP_PDM_NUMBER))=
?_FORMAT_0("<ATTR(ERP_PDM_NUMBER)>").toFileName("_").add(".ipt").value()