![]() |
4.19.
Further settings in "plinkgroups.cfg"
4.19.3.
Adjust Standard name -
Standard name (short) - BOM name / plinkcommon.cfg -> Block
[PARTdataManager] -> Keys "NB" "ShortNB" "LINA"
|
|
---|---|
Prev | Next |
![]() |
Important |
---|---|
Files names for the exported CAD document should be absolutely unique. The entire CAD
administration, including definition of name rule, is performed via CAD
configuration files under Detailed information on CAD administration in general can be found under Chapter 2, PARTsolutions - CAD Integration - Administration. Detailed information on creating the file name in particular can be found under Section 2.2.2, “Set file name ("FileName" key) and pool path ("poolpath" key) ”. By default, on
the tabbed pages Standard name,
Standard name (short) and BOM name, NO entries are performed! Then in
PARTdataManager, in
the 3D view, the standard NB and in the table docking window the
standard LINA is displayed and the setting under
If entries have
been performed on the tabbed pages Standard name, Standard name (short) and BOM name, then will change the NB! This again
effects the setting under |
You can find the same setting options both in PARTlinkManager and in PARTadmin. The syntax is identical.
Also see Registerseite Standard name , Standard name (short) , BOM name .
![]() |
Note |
---|---|
The same
keys are found in the configuration file |