![]() |
4.2.5. Configure the
data-source for ODBC (exemplified by MSSQL)
4.2.5.1. Database connection via file DSN
|
|
---|---|
Prev | Next |
Alternatively you can set up a database connection via File-DSN.
A central place for saving connection data. Changes only need to occur in this place during database or computer changes!
Example using the database server MySQL:
First create the
file mysql_filedsn.dsn
in the $CADENAS_DATA
directory.
[ODBC] DRIVER=MySQL ODBC 3.51 Driver Description = PARTsolutions - intelligentes Teilemanagement SERVER = \\yourDBServerName.yourDomain PORT = USER = root Password = Database = partlinkdb OPTION = 3 SOCKET =
In the ODBC data source administrator the file shows up in the DSN file rider:
Configuration in PARTsolutions:
Extras -> Configure ERP environment -> Rider Database -> Field Database.
Name such as $CADENAS_DATA can also be used in the path.
In PARTlinkManager, in the lower left corner, the following shows up after successful connection: Connection established.