Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Comments on the single setting options are found in the configuration file itself. In the following only an overview on the most important settings is given.
The settings are performed in the
configuration file ifprofile.cfg
.
Here details on the PRO.FILE checkin can be set, among others the parameter WORKFLOW_STATE_CREATE, which has to be adequate to the specified workflow final state in PRO.FILE (compare Section 3.3.6.4, “Settings within PRO.FILE”).
Declaration of the used CAD system
The declaration of the CAD system, which shall be used together with ProFile, happens via coding scheme by the following values:
CADSYSTEM=33
(See PRO.FILE database table 'CADVERS' fields VE_TYP and VE_REL: 4=ProE, 33=Inventor, 21=SolidEdge, 25=SolidWorks)
Enter the version of the CAD system.
CADVERSION=2011
Determine the workflow status for new created parts.
WORKFLOW_STATE_CREATE=100
You can find the respective status in PRO.FILE under File --> Verwaltungsfunktionen --> Workflow --> Berechtigungstabellen verwalten.
Section [CreationOptions(is3d)]
Searching for already existing parts?
0: A new part is always applied.
In order for the ERP number to be inserted into this part, the key OVERWRITE_EXISTING_PARTFIELDS has to be set on 1.
Furthermore an entry for the ERP number has to be set in the section [AttributeMapping].
[AttributeMapping(is3d)] NFT_FLO0=?GetObject("iface.calcnameservice").start(0).Format ("<ATTR(ERP_PDM_NUMBER)>").value() )
1: When creating new CAD documents it is searched for already existing part in PRO.FILE.
Then the new document is linked with the found part (same ERP number).
If no part is found, then a new one is created (new ERP number) and the document is linked with it.
Overwrite existing "partFileds"?
Determine storage location for ERP numbers
PROFILE_ERPField=NFT_FLO0
Here the column name in the PRO.FILE database can be stated, where the ERP number is saved.
PARTsolutions_ERPField=?GetObject("iface.calcnameservice").start(0). Format("<ATTR(ERP_PDM_NUMBER)>").value()
Here the PARTsolutions ERP number is read. In the example it is saved in the column "ERP_PDM_NUMBER".
0: Old parts get the workflow status of the new document, which is linked with this part.