Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
2.3.6.2. Block
[INTERFACE]
2.3.6.2.1. Key
"PhysicalPropertiesPrecision" - Allow physical property precision
override
|
|
---|---|
Prev | Next |
The current "0.99999" precision level for physical properties provides adequate accuracy for PARTsolutions software needs (particularly volume unit conversion), however, for certain NX models the calculation of these properties takes an extremely long time.
The key
"PhysicalPropertiesPrecision
"
provides the possibility to reduce the precision to an acceptable level
(NX UI default is 0.99).
Default value is "0.99999", meaning the physical property precision is five decimal places. The user can now change this precision by adding or removing the "9"s in the string. A precision of "0.99" offers a "good enough" approximation and speeds up the calculation dramatically.