Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
ODBC connectivity to the database system regarding software and license has to be ensured by the customer.
In the following setting up the ODBC data-sources is explained exemplarily for MSSQL. The description also applies for other database types. Precondition is an ODBC driver compatible with the used database.
Run the ODBC data-sources (preferably directly via exe file, in order to avoid conflicts due to the architecture).
Under System DSN add a new data source.
For the driver select SQL Server and confirm with .
Enter Name, Description and Server address of the data source and then click on .
Perform settings in the dialog box Create a New Data Source to SQL Server according to the following figure.
If now a connection error occurs, regard the following notes:
Now change the default database to the just created and click on .
In the next dialog perform the desired settings and click on .
The result should look like this: