powered by CADENAS

Manual

Manual

4.2.4.3. Additional functionalities

  • ERPADDTABLE

    This table is only necessary for connection of ERP systems.

    When transferring values, a field with a specific variable value is added.

  • MAPPING

    This table is only necessary for connection of ERP systems.

    Here a description between the descriptions in PARTsolutions and those in the ERP system is created.

    Adjustment is customized.

  • NBTABLE

    If the originally formed file name is too long, a replacement is given.

    The table secures the unique allocation of the changed file names.

    Adjustment is customized.

  • REPLACE_TABLE

    When opening certain standard or supplier parts, a window shows up in which references to other parts are listed, which can be loaded instead of the original selection. The table serves as allocation table.

    Optionally, concerned parts may be identified with a symbol in the PARTdataManager directory tree.

    Old standard cancelled without replacement

    Old standard replaced by at least one other parts family

    Old standard replaced by at least one other parts family and old standard locked

    Symbols - directory tree

    Symbols - directory tree

    Detailed information can be found under Section 1.7.3.3, “ replace_std.cfg ”.