Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
5.8. Table layout for
PARTdataManager and (PARTlinkManager)
5.8.2. Tabellenwerte anpassen
-> Farbe anpassen / plinkcommon.cfg -> Block
[COLMAPPING_<variable name>] - Key COLORCODE<Nummer>
|
|
---|---|
Zurück | Weiter |
With the help of the option Farbe anpassen you can set internal values to be displayed in different colors.
The setting applies for PARTdataManager and PARTlinkManager as well.
Setting in
configuration
file $CADENAS_SETUP/plinkcommon.cfg
:
Block [MAPPING_<variable name>], key COLORCODE<NUMBER>, first internal value, then values for RGB code
[COLMAPPING_ACTIVE_STATE] COLORCODE0="0","255","0","0" COLORCODE1="1","0","255","0" COLORCODE2="2","0","0","0"
Setting in user interface under PARTlinkManager -> Extras menu -> Konfigurieren dialog box -> PARTlinkManager Einstellungen tab -> Tabellenwerte anpassen -> Farbe anpassen:
Exampe for ACTIVE_STATE: The first values stand for locked (0), released (1) und expired (2). The following values stand for the desired color in RGB code. The setting applies for PARTdataManager and PARTlinkManager as well.
Zurück | Nach oben | Weiter |
5.8.1. Tabellenwerte anpassen -> Text anpassen / plinkcommon.cfg -> Block [MAPPING_<COLUMN_NAME>] - Key for visible text | Zum Anfang | 5.8.3. Tabellenwerte anpassen -> Text und Farbe anpassen / plinkcommon.cfg -> Block [MAPPING_<variable name>] -> Key for visible text |