Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
5.8. Table layout for
PARTdataManager and (PARTlinkManager)
5.8.3. Tabellenwerte anpassen -> Text und Farbe anpassen / plinkcommon.cfg ->
Block [MAPPING_<variable name>] -> Key for visible text
|
|
---|---|
Zurück | Weiter |
With the help of the option Text und Farbe anpassen you can set text to be displayed in different colors.
The setting applies for PARTdataManager and PARTlinkManager as well.
Setting in
configuration
file $CADENAS_SETUP/plinkcommon.cfg
:
Block [MAPPING_<variable name>], key stands for the displayed text, first value stands for the internal value, next values stand for the color in RGB code.
[MAPPING_ACTIVE_STATE] Locked="0","255","0","0" Released="1","0","255","0" Expired="2","0","0","0"
Setting in user interface under PARTlinkManager -> Extras menu -> Konfigurieren dialog box -> PARTlinkManager Einstellungen tab -> Tabellenwerte anpassen -> Text anpassen:
Zurück | Nach oben | Weiter |
5.8.2. Tabellenwerte anpassen -> Farbe anpassen / plinkcommon.cfg -> Block [COLMAPPING_<variable name>] - Key COLORCODE<Nummer> | Zum Anfang | 5.8.4. Tabellenwerte anpassen -> Farbe mit Bedingung anpassen / plinkcommon.cfg -> Block [COLMAPPING_<column name>] -> Key "COLORCOND<Nummer>" |