Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
Special license needed (PSDEV*PIDENT)
Support only through CADENAS consulting team
You can transfer any information from third party systems to PARTsolutions (with ERP integration) into the link database cyclically.
This config will be used during the nightupdate of ERP data.
Setup a scheduled task/cronjob with this command:
"%cadenas%\bin\x86\32\cscripthost.exe" "%cadenas_setup%\scripts\erp\nightupdate.vbb"
In the following you can find details on the single blocks and keys.
![]() |
Hinweis |
---|---|
Zur Aktualisierung des Suchindex finden Sie Informationen unter Abschnitt 5.5.9, „Weitere Informationen“ -> "Automatische Index-Updates". Ein veraltetes
Konzept ist das Update per Scripting durch |
![]() |
Hinweis |
---|---|
Also see Abschnitt 5.13.3.3, „Daten automatisiert und zyklisch aktualisieren - “. |
Zurück | Nach oben | Weiter |
1.1.6.7.14. material_assign.cfg (mit ERP-Kopplung) | Zum Anfang | 1.1.6.7.15.1. Block [LOG] |