powered by CADENAS

Manual

Manual

8.6.2.1.1. Manuel Input

  • Classification: select the desired classification.

  • Extract classification number from

    • Activate the option Input.

      Click the browse button ....

      --> The Classification window opens.

[Note] Note

Pay attention to the following difference!

  • Define Classification Number

  • Add classification number

Via the option "add" you can successively take up allocations via different levels.

Window: Set classification

Window: Set classification

Window: Classification

Window: Classification

Take up all allocations, as described under "Zuweisung auf Projektebene" .

Confirm with OK under the Set classification window.

--> All projects of the selected directory are accordingly classified. In the Create standardization system window the allocations are listed.

At the end of the process, you receive a corresponding message with the advice to conduct an update in PARTadmin.

Window: Create standardization system

Window: Create standardization system