powered by CADENAS

Manual

Manual

8.6.1.1.  Allocate classifications

PARTproject should insert a part into a classification, assign it an attribute, and display the result in the PARTdataManager.

  1. Click on the project file of the part, that you want to classify.

  2. Click on the browse button ... in the Classification ('name') field of the desired classification.

    --> The Classification window opens.

  1. Choose the corresponding directory into which the selected part should be inserted.

    [Note] Note

    The search function is helpful to quickly find the correct directory. The search may be carried out by clicking on the Search or by pressing the Enter key.

    If you select a search result, the tree at the right will be expanded and the respective item is selected.

    Double-clicking a result causes it to be added directly to the Selected classes area. (Otherwise you need to specifically add it using "Add".)

  2. Order the classes (or the insertion point) per Add button .

    Or double-click on a search result to add it to said class.

  3. Close the window by clicking OK.

  4. Save the changes.

  5. [Note] Note

    Only after an Index update in PARTadmin (see Section 1.1.3.4, “ Index administration ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual) will the result be visible in the PARTdataManager.

--> In the classification ('name') field, the class ID of the selected directory appears.

A classification can be planned for parts, as well as for Connection points .

In case both options are possible, select the option Classes or Connection points before allocation in the selection list under Filter (see figure below).

The most classes only have the Classes option is available.

Classification window: Adjust size of individual dialog areas if desired.

Classification window: Adjust size of individual dialog areas if desired.

The Classification window can be reached via the context menu of the directory tree via Add projects to classification.

For more information see the next section under Section 5.6.2, “Allocation at directory level”.

The context menu command Add projects to classification is available at project level, as well as at directory level.