Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Sweep is the transition between two sketches on parallel planes and the same number of sketch elements.
With V10 Sweep is released as a standard function.
In the part EN 10253 for example, the sweep function is used.
In the following you can see an excerpt in PARTdesigner, which exemplifies the usage.
Create a circle in a base sketch.
Create a parallel reference plane with the desired distance and on it a new sketch.
On sketch 2, in the same way, create a circle again. (Here in the example it is smaller and shifted in relation to the first circle.)
Mark both sketches under History and then click on Create sweep base.
-> The dialog box History opens.
-> The sweep is displayed in the 3D view.