Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
By simply clicking on the menu item Insert part..., theOpen file dialog pops up. Select a Project file (*.prj). |
Before the configurator tree is expanded with the selected part, a query for the Part properties takes place. Set these. |
Note | |
---|---|
You may also define more parts as start elements! Important! See also Section 9.8, “Example 2 - Create an Assembly-Table-Project ”. |
Fully positionable : Part cannot only be positioned via connection points, but must also have vector description to a specific location in space.
Note | |
---|---|
The z-axis field is not needed since this value is automatically calculated. Incorrect entries in the y-axis section are automatically corrected. |
No export : During export of the table from PARTdataManager to a CAD system this part is not exported
Parts with the option No export , contain in the PARTdataManager, in the dialog area Assembly, Bill of material the icon NO CAD (see image at right).[a] |
|
[a] Compare alsoFenster "Aufbau" - Stückliste. |
Transfer to Bill of Material: The respective part is taken over by PARTbom order list (see Section 9.5.2.2.3, “ Transfer to PARTbom ”).
Parts without the option "Transfer to Bill of Material " show up grayed in the PARTdataManager in the dialog area Assembly, Bill of material (see image at right: "NO BOM").[a] |
|
[a] Compare also Section 3.1.2.7.15, “"Assembly" Window - Bill of material Window ” in PARTsolutions / PARTcommunity4Enterprise - User manual. |