Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
These symbols signalize general changes:
? = directory / project unknown in version management
Arises when changes are made in Explorer, thus outside of PARTproject.
Occurs if a directory has been edited by another user in the meantime.
Occurs if two users changed the same file at the same time. This case should be avoided! And if it happened, you can find help under Section 6.15.1, “ eCATALOGsolutions: PARTproject QA - Solve SVN conflict”.
V = Subversion conlict of versions
Local working copy has to be updated to V10. See Section 6.2, “Installation QA Module ”.
- = Subversion difference in versions
If a V9 is accessing catalogs/projects which have been edited with V10 then a minus icon is displayed.Section 6.2, “Installation QA Module ”.
The same symbols are also used in the Send changes to the server dialog.