If you want to export special derivations into the CAD system later, then proceed as follows:
Call PARTdataManager via PARTsolutions menu -> Insert 2D (Insert model).
Call up export function:
The further process depends on the setting under Extras menu -> Settings... -> Export to CAD. See Section 12.1.12, “"Export to CAD" tabbed page ”.
Directly after having selected the desired part, click on Transfer to CAD .
-> The dialog box Choose view to pass... opens.
Dialog box "Choose view to pass..."
Select the desired derivation and confirm with OK.
-> The derivation is directly transferred to CAD.
Click on the button 2D derivation .
-> The docking window 2D derivation is opened.
2D derivation
Select the desired derivation.
Click on Transfer to CAD .
Result:
Result exemplarily in AutoCAD