With the Configurator, parts - created in PARTdesigner - can be connected to complex Assemblies.
The control of the assembly configuration is determined via a system of rules.
The following is determined there...
...which connection parts for the Start element will be available in the PARTdataManager,
...at which locations these parts are added to the start element
...and how the selection of the respective table will be dimensioned.
Independent PARTdesigner parts without system of rules
Built up assembly with system of rules
Parts can only be configured to an assembly if Connection points have been assigned in the PARTdesigner before!
In the Configurator a Set of rules is later created which connects parts according to their Connection points.