Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Each dimensioning must contain the following parameters:
ID is only required, if a dimensioning serves as Base dimension for a chain dimensioning.
The description is shown in the above listing. Initially a description is automatically given, when creating a new dimensioning, which can be adjusted as desired.
When creating a new dimensioning, HORIZONTAL is displayed initially. In the list field, adjust the selection to RADIAL. You can change the type anytime.
At the desired 2D views, where the dimensioning shall be displayed, activate the checkbox.
Views which
contain a dimensioning, can be recognized in the 3D toolbar, by a
respective icon with dimensioning lines .
Select a Connection point as center of the circle of the radial dimensioning.
(The measuring distance [see next point] determines, where the arrow is visibly inserted.
Measuring distance is the aiming point of the arrowhead (normally the circle radius, because otherwise the arrowhead would have no real focus).
Specify a fixed value or better a variable.