![]() |
Sometimes it makes sense to temporarily disable one or several sketches (Base extrude / Cut extrude) (e.g. for testing purposes).
For this use the function Deactivate / Activate. You can apply it for a single sketch and for several all at once just as well.
When using Deactivate there are two possibilities:
In order to activate proceed the other way around.
Hidden "Base
extrudes" are marked with a respective icon .
Sketches with
condition are marked with the "if" Icon by default.
![]() |
Note |
---|---|
The new
feature is fully compatible with older versions, just the icon
|
Initial situation: For sketch 3 a condition exists, for sketch 2 not. Both shall be hidden.
Mark the desired Base extrudes and click on context menu command Deactivate.
-> Hidden
"Base extrudes" are marked with a respective icon .
-> By default, the sketches are
marked with the "if" icon.
Open Base extrude 2. The invalid condition "0=1" has been entered.
Open Base extrude 3. Here, the invalid condition "0=1" has been concatenated with the already existing "C=6" using "&".
In order to enable the sketches again, click on the context menu command Activate.