![]() |
5.10.7.
Optional parameters Details
5.10.7.1. Correct display
of inch variables in dimensionings
|
|
---|---|
Prev | Next |
As of V11 SP9 decimal values in dimensionings can be displayed as fraction.
For this use following expression:
%frac%[accuracy]
"{0.75%frac%2}" is displayed as "3/4".
Mixed text for dimensionings is also possible:
"{0.75%frac%2} = {0.75}" is displayed as "3/4 = 0.75".
![]() |
Important |
---|---|
The accuracy of values determines how many decimal places will be considered. So "{0.75%frac%1}" is displayed as "4/5", because 0.75 is rounded to 1 decimal place (0.8 -> 4/5). |
Maximum value for accuracy is 9. Higher values are set back to 9 internally.
If a part is opened in a version that does not support fractions, the decimal value will show up.