![]() |
= gleich <> ungleich > größer < kleiner >= größer gleich <= kleiner gleich AND OR
The following examples show key values:
1
ERPTABLE.PRICE<=0.8
The expression is true, if the respective field of the column PRICE has a value lower or equal than 0.8.
LINKTABLE.ERP_PDM_NUMBER<>''
The expression is true, if the respective field of the column ERP_PDM_NUMBER is not equal empty.
(LINKTABLE.ERP_PDM_NUMBER<>'') AND (ERPTABLE.PRICE3>0.0)
The expression is true, if the respective field of the column ERP_PDM_NUMBER is not equal empty AND the respective field of the column PRICE has a value greater than 0, in other words a pricing is available.
((LINKTABLE.ACTIVE_STATE=1) AND (ERPTABLE.STANDORT1<>''))
The expression is true, if the respective field of the column ACTIVE_STATE has the value 1 (= released) AND the respective field of the column STANDORT1 is not equal empty, in other words has an entry.