powered by CADENAS

Manual

Manual

5.8.2.2.11.1.  Save as CIP
  1. Mark the required project and click on the context menu command Save as CIP.

    -> The dialog box Create CIP file is opened.

  2. Settings:

    • CIP file to create: Apply the path in which the *.cip file will be temporarily stored.

    • Part directory: The path of origin of the project is entered per default. If you do not change it, the *.cip file is then placed into this path when starting.

[Note] Note

When opening the *.cip file, the PARTdataManager is automatically started. The cipped part is imported into the directory tree and the index is automatically created.

In PARTproject the cipped file is only visible after restarting the program.