Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Within architectural / BIM catalogs the topic LOD (Level of Detail) is especially important - parallel to the known „mechanical LOD’s“ high / medium / low for AEC / BIM an own system is existing with the schema 100 / 200 / 300 / 350 / 400 / 500 – this will be described further below. Beside LOD (=Level of Detail) often the terms “Level of Development” or “Level of information” (=LOI) occur in the BIM market. In the CADENAS catalogs these concepts were put together.
When creating a new project, please use the template Template for 3D project with LOD
or Template for 3D project with LOD (AEC – Z-axis on top) (default Architecture) / Template for 3D project with LOD (MEC – Y-axis on top) (default Mechanical).
In doing so the LOD control variables are created in PARTdesigner „by default“ and later will be available in PARTdataManager.
|
If an existing project should be extended with the LOD control variables, please right-click on the project / folder in PARTproject and run the command Automation > Add LOD Variables. (By default, available in V11 or as of V10 SP10 after installation of a special plugin. Should you need this plugin, please write an e-mail to catalogs@cadenas.de.)
In the following window you can select which LOD levels should be set up for mechanical or architectural target systems.
Further below in this document you will find assistance if you are not yet familiar with the selection of LOD levels.
|
Via both ways in the project table, the two LOD control variables LODDEST and LODLEVEL will be available:
With the variable LODDEST at first the primary target market can be selected
Depending on this, the value range LODLEVEL will show the known levels high / medium / low from mechanical market or the stages 100-500 from the architectural branch (depending on how many stages were set up).
In the further creation process, the modeler has to connect the different detailed models with the corresponding LOD stage by himself. This will happen with known and existing eCAT features.
The LOD*** algorithms, which also will be added automatically in the project table, have to remain untouched.
The LOD definition is a very big knowledge and discussion ground. It is not target of this guideline to give an overload of information – instead of it a very simple instruction / imagination shall be given on how to set up the LOD levels for MEC / AEC.
AEC LOD 100 | |
AEC LOD 200 | |
AEC LOD 300 = MEC LOD Low | |
AEC LOD 350 = MEC LOD 350 | |
AEC LOD 400 = MEC LOD High | |
AEC LOD 500 / 600 / 700 |