Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In this section you can find details on the setting options of Text .
General: See Section 14.4.2, “General settings”.
Language: This function is not available currently. Apply translations in PARTproject as described. On this see under Section 14.7.2, “Translate Media Variables ”.
Font: The font types, available in the system are displayed in the list field.
| ||||
[a] $CADENAS_SETUP/datasheet/fonts |
Standard paragraph format / List formats:
In the list field of the paragraph formats you can find options like Standard, different bulleted list formats or numbered list formats. Via the little list field to the right you can control the indentation level (starting with 0 = no indent).
It is possible to use variables as text:
Project variables such as "$NB.", "$NENN.", "$LINA." for example
Media variables: On this see Section 14.6, “Edit Media Variables in the Media editor ”.
Special variables, which can be inserted via context menu. These are marked with "$$" (Example: $$MASS$$).