The
PARTserver dialog area is displayed
at directory and project level.
PARTserver
preview:
May be selected at project and
directory level.
As the preview (see illustration
at right), the katalog.bmp set in the Image tabbed page
box is displayed in PARTserver/PARTcommunity (online
catalog system). If you wish to set a differing preview,
enter this in the PARTserver
preview field.
Note
In order to delete the set preview,
it must be deleted manually from this field.
Thumbnail for
PARTserver:
Part image (2D and/or 3D) within
the PARTserver/PARTcommunity detail level. (Project
level)
Additional
files:
Visible
at directory level.
Enter
those files here that should be copied after
PARTserver/PARTcommuntiy. Per default the add-on ",0" is
added.
Should
an entire subdirectory need to be copied (for ex., needed for
assistants) however, then specify the subdirectory and change the
parameter to "1".