powered by CADENAS

Manual

Manual

7.8.2.2. Settings for the catalog

[Note] Note

This dialog area is now displayed on catalog level.

  • Catalog name

    This description shows up in the PARTdataManager.

  • Private catalog

    Value range: Yes / No

    Private catalogs cannot be published and furthermore for these no icons concerning publishing will be displayed. Detailed information on catalog publishing is found under Section 9.10, “Publish catalog ”.

  • Subfolders to exclude

    If you want to exclude certain directories (e.g. print data) from the cip generation, then proceed as follows:

    1. In PARTproject, on catalog level, call up the tabbed page General1.

    2. Under Settings for the catalog -> Subfolders to exclude click on the search button ....

    3. -> The dialog box Select subfolders to exclude opens.

    4. Activate the checkbox at all directories to be excluded and confirm with OK.

    5. -> The selected subdirectories are inserted separated by comma.

  • Name of installation

    You can assign your own description for the installation process.

    Name of installation

    Name of installation

    You can also store translations on the Translation tabbed page for this.

    Name of installation

    Name of installation

    The term entered under Name of installation will be displayed during installation in PARTadmin or during installation of the DVD.

    Name of installation

    Name of installation

  • Catalog created in the language

  • Catalog available in the languages

    Define translation languages

    Define translation languages

    The translation languages are displayed on the Translation tabbed page.

    [Note] Note

    A detailed description for the catalog translation is found under Section 7.7.2.1.13, “ Translation ”.

  • QA

    If a catalog that is QA managed should be created, then you must select Yes from the list.

    Detailed information about PARTproject QA can be found under Chapter 6, PARTproject QA.

  • Server

    For SVN managed catalogs, the entry occurs automatically.

  • Download additional QA files

    Currently not being used.