Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This command provides an alternative to value range variables. Using Duplicate line, you can subdivide an attribute (table row) into various sub-attributes if, for instance, the contents of only one column are to change.
In the example below, there is a component with three different attributes (rows). The value of variable B has the constant dimension of 1 mm. The existing three rows are now to be duplicated and, at the same time, the value for B in the new rows is to be changed to 2 mm.
Choose the variable (in this case "B") whose column value(s) is (or are) to be duplicated.
Click on the Add valuebutton. --> The window of the same name is displayed.
Enter the variable value (in this case "2") for the new/duplicated rows. --> Each row of the table is duplicated and the new variable value (in this case "B" = 2 mm) is entered.