Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Here you can define, how the classes of the two class systems shall be compared to each other.
Options for the class mapping:
In the list field select the desired method:
Select that method with which presumably the most defined mappings can be made. Single entries in the result can later be reworked with another method. See Section 5.13.13.3, “Edit mapping”.
Maximum character distance: The entered number determines the number of maximal allowed different characters between two field entries.
Options for the class variable mapping:
Here you can find the same setting options as under Options for the class mapping.
After a certain processing time (depending on the size of the classifications) the result is displayed in the dialog box pproject.