As you know, Discord may be a great platform where you can connect with your friends, colleagues, and enjoy seamless communication with them over a private channel. Initially, Discord was built for meetings purposes since it's lots of cool features like screen sharing, voice calling, texting and video calling as well. However, one of the most useful features of Discord is that you can create a channel and engage with a much larger audience. Generally, it's quite easy to attach to someone’s voice server. But recently, most customer have been complaining about the RTC connecting no route discord error. Mainly, this particular “discord rtc connecting no route” occurs when Discord is unable to create a proper connection with the server and eventually faces problems while connecting to it due to some network issues.
Disable VPN
One possible reason for the Discord RTC connecting no route error can be some VPN service you might be using on your pc. Since Discord servers operate after checking on the User Datagram Protocol (UDP), most VPN servers do not have that functionality. As a result, the discord app faces problem while connecting to the channels and cause such an error to occur on the system.
Hence, for this Discord no route fix, the simplest method isn't to use any VPN service at all. Otherwise, if you still want to use a VPN on your device, you must ask your VPN provider to enable UDP, or maybe find another VPN provider that gives UDP with servers by default. Both the options will work best for you, but as our personal opinion, we would suggest you not to use one because it can also cause some other kinds of errors with Discord or other applications.
Disable Quality of Service High Packet Priority in Discord
Step 1. Launch Discord on your Computer.
Step 2. Click on the Settings icon which is present right beside your avatar in the bottom left corner of the screen.
Step 3. In Settings, click on Voice & Video in the left pane.
Step 4. Here, you will find the option that says, Enable Quality of Service High Packer Priority. make sure to keep it disabled.
Step 5. Now, restart Discord and try to connect to the channels again and see if the error is resolved or not.
As you know, Discord may be a great platform where you can connect with your friends, colleagues, and enjoy seamless communication with them over a private channel. Initially, Discord was built for meetings purposes since it's lots of cool features like screen sharing, voice calling, texting and video calling as well. However, one of the most useful features of Discord is that you can create a channel and engage with a much larger audience. Generally, it's quite easy to attach to someone’s voice server. But recently, most customer have been complaining about the RTC connecting no route discord error. Mainly, this particular “discord rtc connecting no route” occurs when Discord is unable to create a proper connection with the server and eventually faces problems while connecting to it due to some network issues.
Disable VPN
One possible reason for the Discord RTC connecting no route error can be some VPN service you might be using on your pc. Since Discord servers operate after checking on the User Datagram Protocol (UDP), most VPN servers do not have that functionality. As a result, the discord app faces problem while connecting to the channels and cause such an error to occur on the system.
Hence, for this Discord no route fix, the simplest method isn't to use any VPN service at all. Otherwise, if you still want to use a VPN on your device, you must ask your VPN provider to enable UDP, or maybe find another VPN provider that gives UDP with servers by default. Both the options will work best for you, but as our personal opinion, we would suggest you not to use one because it can also cause some other kinds of errors with Discord or other applications.
Disable Quality of Service High Packet Priority in Discord
Step 1. Launch Discord on your Computer.
Step 2. Click on the Settings icon which is present right beside your avatar in the bottom left corner of the screen.
Step 3. In Settings, click on Voice & Video in the left pane.
Step 4. Here, you will find the option that says, Enable Quality of Service High Packer Priority. make sure to keep it disabled.
Step 5. Now, restart Discord and try to connect to the channels again and see if the error is resolved or not.
Without any route error now it has become easier for everyone to fix the RTC connecting easily. Such technical errors are common to occur. And we can use best essay review to get rid of these issues easily. But the best thing is they always try their best to sort out these issues in a positive and best way.
Without any route error now it has become easier for everyone to fix the RTC connecting easily. Such technical errors are common to occur. And we can use best essay review to get rid of these issues easily. But the best thing is they always try their best to sort out these issues in a positive and best way.