The Alfa Romeo MiTo, a sleek and stylish supermini, has gained popularity since its launch in 2008. However, like any other car model, it has its fair share of reported problems. In this article, we will explore some of the common issues that drivers have reported with the Alfa Romeo MiTo, along with the average cost of repairs and the model's reliability.
Timing Chain Problems
One of the known issues with the Alfa Romeo MiTo is problems with the timing chain. Drivers have reported a rattling sound coming from the timing chain, especially when starting the car. This sound can sometimes persist even after the engine has warmed up. The MiTo's timing chain is more prone to stretching, leading to the rattling noise. If left unattended, the timing belt may snap, causing significant damage to the engine.
It is crucial to address any potential timing chain problems promptly. If you notice a rattling sound or the check engine light illuminates, it is recommended to take your MiTo to a mechanic for inspection. The average cost for a timing chain replacement is around £414.73.
Gearbox Problems
Another commonly reported issue with the Alfa Romeo MiTo is gearbox problems. Many drivers have complained about a noisy gearbox, particularly in higher gears. The sixth gear of the MiTo is prone to rapid wear, resulting in a noisy gearbox. If left unaddressed, this issue can lead to severe damage, requiring a complete gearbox replacement.
If you are experiencing gearbox issues, it is advisable to have it repaired as soon as possible. The average cost for a gearbox repair on an Alfa Romeo MiTo is approximately £465.
Turbo Problems
Drivers have also reported problems with the MiTo's turbo. The turbo seal is prone to failure, resulting in a noticeable loss of power during acceleration. You might also observe slow and noisy acceleration, black smoke from the exhaust, and the check engine light illuminating on your dashboard.
To prevent further damage, it is essential to have any potential turbo faults examined promptly. Turbo replacement can be costly, with an average quote of £979.76 for an Alfa Romeo MiTo.
Steering Problems
The Alfa Romeo MiTo has been associated with steering issues as well. Some drivers have encountered heavy steering or a complete loss of steering power on certain occasions. You may only notice this problem when the power steering light becomes illuminated.
It is crucial not to ignore steering problems as they can lead to permanent damage to your vehicle. If you experience any steering-related issues, it is recommended to take your car to a local garage or mobile mechanic for inspection. The average cost for power steering repair on an Alfa Romeo MiTo is approximately £107.87.
Recalls
Due to some of these reported problems, Alfa Romeo has announced recalls for affected MiTo models. Below is a table summarizing the recalls:
Affected Model Dates Issue September 2010 - December 2015 The airbag may not correctly deploy, or deploy at all due to a fault with the airbag propellant system Reliability of the Alfa Romeo MiTo.
When it comes to reliability, the Alfa Romeo MiTo has received mixed reviews. In CarBuyer's 2016 Driver Power owner satisfaction survey, the MiTo ranked a disappointing 145th out of 150 cars in terms of reliability. Although more recent models show some improvement, it still falls somewhat below par.
One contributing factor to the lower reliability score is the absence of a low-speed collision mitigation system, which many other small models in the same price range offer. However, the Alfa Romeo MiTo did achieve a five-star rating for adult safety protection from Euro NCAP. Child and pedestrian safety were rated three and two out of five stars, respectively.
Thanks for giving your valuable time to read this blog, If you have a car and wondering, how to find a car service center for my car ac gas refill service? Open Google and type
car ac gas refill near me and you will find the Service My Car website on the top of SERP to get the best car ac gas refill service in your area.
Conclusion
Despite its sleek appearance and style, the Alfa Romeo MiTo has encountered several common problems reported by drivers. These include timing chain issues, gearbox problems, turbo failures, and steering difficulties. It is crucial to address these problems promptly to prevent further damage and costly repairs.
When considering the reliability of the MiTo, it is important to note its lower ranking in terms of reliability compared to other models. However, it still boasts excellent adult safety protection ratings from Euro NCAP.
If you own an Alfa Romeo MiTo and are experiencing any of the reported problems, it is advisable to consult a trusted local garage or mechanic for the best price and service. Remember, regular maintenance and prompt attention to any issues can help ensure a smoother and more enjoyable driving experience with your Alfa Romeo MiTo.