Amazing Hologram Effect!
Add me on Facebook. (click LIKE on Facebook to add me)
http://www.facebook.com/brusspup
Download the song in this video:
Song name: Soul Switch
https://itunes.apple.com/us/album/soul-switch/id426471027?i=426471065&ign-mpt=uo%3D4
http://www.amazon.com/Soul-Switch/dp/B005HMR1LM/ref=sr_1_1?ie=UTF8&qid=1354354756&sr=8-1&keywords=brusspup
For more information about the product (Giant Mirage) visit their website:
http://www.optigone.com/#GiantMirage
My channel was recently featured on Kids React. Check it out here:
http://www.youtube.com/watch?v=ZrsO6svChTs
This device is amazing. It works exactly like the smaller units that have been around forever. But with the Giant Mirage you can put much larger objects inside. The effect in person is stunning. It really looks like the object is floating in mid-air. The effect is so powerful, it almost makes you dizzy when you walk around while looking at the object.
The device works by using a mirrored surface on the inside. When you place an object inside and step back and look at the opening, you're seeing a "double" reflection of the object. From the person's point of the view, the object is first reflected in the top mirror, then it is reflected to the bottom mirror, which is the final image that you see.
Posted March 12, 2016
click to rate