Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Add class allows you to add further classes or subclasses into the already existing structure.
Note | |
---|---|
In order to add classes, do the following:
Mark the class under which you would like to add another class.
-> The same-named dialog opens.
The fields Name, Description and Path are automatically filled. The data are read from the calling class. When you change the class in the index tree and call up the command again, then the data is updated.
Under Description enter the language specific name. If an entry exists here, then it is used, otherwise the entry under Name.
Note | |
---|---|
When you add a subclass to a class which already contains parts (datasets) then these are not visible anymore or even deleted. The concrete behaviour depends on the configuration. You can find detailed information hereto under Section 2.2.15, “Special hints for adding and deleting classes”. |