Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
You have the option of filling the column ERP_PDM_NUMBER with a timestamp number.
As soon as you have entered a name under ERPNOFIELD, the function is activated.
[CLASSIMPORT] ERPNOFIELD=ERPNO
In addition, the following adjustments must be made:
In the
[MATNR_FIELDS] section under ERPNOFIELD set the declared column here and
allocate the corresponding one from the import file erpdata.txt
.
[MATNR_FIELDS]
ERPNO=1
MAT_NAME=2
DESCRIPTION=4
Note | |
---|---|
Make sure that the referenced column in the LinkDB really does exist. Whether or not the column is to be displayed in the PARTdataManager as well, depends on the role configuration. |
The entry is composed of the current time "%time%" and a numerical value "%var%".
MINSIZE determines the number of places and MINVALUE the Start value for the numerical value.
[TIMESTAMP] TEXT=%time%.%var% MINVALUE=1000 MINSIZE=5