powered by CADENAS

Manual

Manual

1.1.5.6.2. Import STL files

There are two different configuration options for importing STL files:

  1. [STLIMPORT]
    OnVariant=0/1

    If you decide on this option, set the value to '1' and OnClass to '0'.

    Use this option, if there is an STL file for each row (article number).

    [Note] Note

    In this case, the columns MATNR, CLASSNAME and STLFILE Fig. „filelist.txt“ are standard and must be filled out. Compare

  2. [STLIMPORT]
    OnClass=0/1

    If you decide on this option, set the value to '1' and OnVariant to '0'.

    Use this option, if there is an STL file for each class.

    [Note] Note

    In this case, the columns CLASSNAME and STLFILE standard and must be filled in; the MATNR field must remain empty.