In the dialog box Edit documents in product you can add geometries, preview images and technical previews.
Complete process exemplified by Add geometry:
Select a product line and click on the context menu command Edit documents in product.
-> The same-named dialog box opens.
Activate the option Import CAD File and click on .
-> The document is inserted in the dialog box Edit documents in product.
Afterwards,
in the product view, click on the button Create geometry and preview from CAD Data.
-> The dialog box Geometry selection opens.
Select the respective option (here exemplified preview image and geometry (.zjv) shall be created only for the selected product) and confirm by clicking on .
-> The dialog box Format Selection opens.
The dialog box for batch export options opens.
Normally you can leave the presettings. Confirm with .
-> In the dialog box Edit documents in product, you can see the following files:
You can recognize the successfully passed through process at the displayed preview image.
For Add technical view and Add preview image the process is similar.
When importing technical previews to a whole class (prj) or a single dataset, you can also use Multipage TIFF and SVG.
The call happens in PARTdataCenter via context menu command Edit documents in product -> Add technical view.
However, precondition is the installation of ImageMagick, with the help of which the added files are converted into the PNG format.
In order to
convert SVG please set the following block in $(Cadenas_user)/partdatacenter.cfg
and adjust the path according to your installation.
[conversion:svg] program=C:\Program Files\ImageMagick-7.0.10-Q16-HDRI\magick.exe %path% %targetpath% format=png
(%targetpath% is a placeholder for the temporary file which is then created by the code.)