Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
Value range fields can also be show in PARTdataManager.
Value range fields can be defined as:
In order for the value range field to be shown in color and work according to plan in the PARTdataManager, you must set the following:
In the columns ATWITHLIST (value list) and ATWITHRANGE (value range) set an 'x' for the desired class name (CLASSNAME) and attribute name (ATTNAME), if you wish to have this function.
If a list of values is desired then apply the corresponding row several times.
In the following figure matnr6 is applied three time with the attribute 'L' (under ATTRIBUTE_NAME). The displayed value is located under ATTRIBUTE_FL_VALUE, since we are talking about a floating number value; with a text the entry must occur under ATTRIBUTE_VALUE.
If a value range is desired, the enter the maximum value in the ATTRIBUTE_FL_MAX_VALUE column.