Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the
$CADENAS_SETUP/classification_toolbar.cfg
configuration file you can make the following settings:
Activate / deactivate the toolbar
initializeToolbar=0/1
Define database login (user and password)
If nothing is set then during launching a respective dialog is displayed.
dbUser=erpuser dbPw=erpuser
Define path for temporary directory
temporaryDirPath=$temp/ct/
Define path
for configuration file classimport.cfg
classimportCfgPath0=$CADENAS_SETUP/classimport_toolbar.cfg
Define path for button scripts in toolbar
scriptsPath=$CADENAS_SETUP/scripts/partdatamanager/classification_toolbar/
You can define whether row-specific preview images should be shown during the geometrical similarity search.
showVariant=0/1
The variable can have the following values:
-2: No messages issued. Special, necessary input dialogs still show up however.
No messages are given but special, necessary input dialogs show up (if "CADENAS_DEBUG = 0",and/or the variable is not set, which complies with the default case).
Special case: If CADENAS_DEBUG =1, the relationship corresponds to "forceDebug = 1" (see next point).
1: Messages are issued and special, necessary input dialogs show up.