Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The file
attributedef.txt
is used for
assembling the tables in PARTsolutions. All Attributes must be described here.
The file contains the following columns:
Al classes and subclasses are listed here.
If a class/subclass contains several attributes (variables), the row is written as many times as needed (in the example "Zylinderschraube" respectively with 'D', 'L', TextA and TextB) (see Fig. „Variables in PARTdataManager“)
Attribute name (variable name)
Contains the names of the attributes [variables] (as many as needed) of the class.
D: Document link[3]
The unit is displayed in the header in PARTdataManager (see Fig. „Variables in PARTdataManager“).
Attribute naming for value range fields
Only needed for value range fields (see Section 2.1.5.5.2, “Value range fields”)
In this case mark the column with an "x". The column is highlighted in orange.
Only needed for value range fields (see Section 2.1.5.5.2, “Value range fields”)
In this case mark the column with an "x". The column is highlighted in orange.
ATBEZ_german, ATBEZ_english, etc.
These columns contain the attribute descriptions in as many languages as you wish.
The attribute description is displayed in PARTdataManager in the column header of the subtitle (for example, length) (see Fig. „Variables in PARTdataManager“).
DISPLAY_VALUES_german, DISPLAY_VALUES_english, etc. (optional)
Optionally contains values of the list fields for the variable search on the Search tab page.
For text attributes which are to be translated, set a '1' in this column. (In the example above at "TextA" and "TextB".)
During the variable search in PARTdataManager the attributes are shown respectively.