Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Via Update ... you can carry out the following operations
First check whether the data of Name, Description and Path is correctly displayed in the Catalog dialog area.
The dialog has the following setting options:
If due to any reasons different file formats of the same type (for Preview, 3D preview or Sketch) exist, you can unitize all file formats with this function. Already existing formats with different file format are converted. The format defined in the configuration file is used.
In order to adjust file formats activate the checkbox.
With the following options you can add some more specifications:
Optionally you can define a start path using the browse button .
Disable automated import of the converted files:
This option is deactivated by default.
If you want to perform a test run without import then activate this option in addition. The result of the test run is found in the "Temp" directory.[10].
Convert regardless of the extension:
Regardless of an possibly already existing correct file format a converting to the target format (according to configuration file) is performed.
When all settings are made click on .
With the dialog is closed without saving any changes.
[10] The
path of the temporary directory is defined under $CADENAS_SETUP/classification_toolbar.cfg
-> section [ClassificationToolbar] -> key
TemporaryPath
.