Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
With the Move datasets command you can move datasets of a project into another project.
First define the source datasets and then the target project.
Open the project where you want to move datasets. -> Now you are in the Part view (table).
Click on Move datasets in the toolbar or in the context menu.
--> The same-named dialog opens.
-> In the Source class dialog Name, Description and Path of source class are already inserted.
Mark (= ) the datasets you want to move via Move datasets -> Select context menu command.
-> On each marked row shows up.
Furthermore in the submenu of Move datasets the following context menu commands are available:
Select the target project in the index tree that is to accept these marked (= ) datasets.
Choose the Move datasets -> Set as target context menu command.
-> Thereby in the dialog window under Target class the Name, Description and Path is inserted.
In the dialog area the table attributes of the project chosen in the index tree are loaded.
In order to change the variables (attribute names) of the target project click into the desired field under Feature name of target project and open the list field with the arrow key.